AXIS#.TEMP

Description

This parameter returns the measured temperature of the power module on the power board for the associated axis.

Examples

Usage

The parameter can be used to track board temperatures as they change during drive operation. There is at least one control board temperature measurement (e.g., DRV.TEMP) and one power board temperature measurement (e.g., AXIS1.TEMP).

Code

--> DRV.TEMP
52.367 (Control) [degC]
--> AXIS1.TEMP
31.664 (Power1) [degC]
--> AXIS2.TEMP
32.312 (Power2) [degC]

Versions

Action Version Notes
Implemented 02-02-02-000

 

General Information

Type

Read Only

Units

degC

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported